Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Il mio contatto
Seleziona luogo

Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.

CH(IT)

Built to last - with drylin W linear guides

Rad9 is THE bicycle shop in eastern Switzerland when it comes to advice, service and high-quality bicycles from well-known brands. The company went in search of suitable assembly stands for their newly erected assembly stations. Although they considered various lifts and assembly stands, none met their specific needs. So they decided to develop a Velolift based on their own specifications. They develop this with our lubrication-free igus products. The MAX Velolift was created with the drylin® W double rail and linear housing.
 

Profile

What was needed: drylin® W double guides and linear housing
Requirements: The lift should be indestructible, strong and beautiful
and be long lasting
Industry: Bicycle industry
Success for the customer: Lubrication-free, strong and long-lasting function
Do you need more information? Contact us here
igus_rad9_application_6

Products used

drylin® W double rail

drylinW_double_rail_icon_website
To the online shop

drylin® W linear housing

drylinW_linear_housing_icon_website
To the online shop

Stepcraft

Problem

The Rad9 company went in search of new assembly stands for the newly created assembly stations. They looked at different lifts and assembly stands, but none met their needs. For this reason, Rad9 decided to build a Velolift according to their own requirements. The company's idea was to develop a Velolift that is indestructible, strong, beautiful and lasts for a long, long time. The two founders then developed the first "MAX Velolift" together with an employee. The prototype worked well the first time, but the design wasn't quite what Rad9 wanted. The ball bearing used always had some clearance and there was a risk of injuring yourself on the guidance or even getting your hand crushed. The two owners showed their prototype to a mechanical engineer who was a friend of theirs, and he recommended that they replace the H-beam with a square tube and the ball bearing with a lubrication-free linear guide from igus.

Solution

Our colleague Axel Ebert from Switzerland visited Rad9 with a bag of samples full of linear solutions. The technical requirements were defined on site, and it quickly became clear to the experienced igus application engineer that the drylin® W modular system was just the thing. Together they decided on the drylin® W double profile guides - two metres long and with a shaft diameter of 20 millimetres, with a guide spacing of 80 millimetres. The ten-millimetre rail would have sufficed, but the price difference was so minimal that the company opted for the more solid version due to its strength, durability and appearance. They also decided on four matching drylin® W linear housings from the modular system. The drylin® W double profile guides are made of hard-anodised aluminium and are therefore corrosion-free. The pillow blocks from the drylin® W linear range are also designed for dry operation and use no lubricants, such as oils or greases. The drylin® W linear product range has many advantages over conventional recirculating ball bearings. No lubrication is necessary, dirt and dust cannot adhere and there is no costly maintenance. MAX Velolift focused on reducing the lift to the essentials. However, this precisely fulfils its function by keeping bicycles permanently strong and safe at the right height.
Stepcraft

gus_rad9_application_12

Axel Ebert, igus Switzerland

"Classic guidance systems have to be lubricated and can get dirty and sticky and later even jam. That doesn't happen with our lubrication-free linear system." - Source: igus GmbH
igus_rad9_application_11

Adrian Schrepfer, Rad9

"We were immediately enthusiastic about the igus linear guide. The operation is extremely quiet and there is no longer any need for the annoying lubrication." - Source: igus GmbH

Further application pictures

_igus_rad9_application_1_ MAX Velolift
_igus_rad9_application_10 The rail system is made of hardened and anodised aluminium - corrosion-free and chemical-resistant



I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH