Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Il mio contatto
Seleziona luogo

Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.

CH(IT)

Energy and signal cable in harvesting technology

Twistable readycable cables as energy and signal supply in ZEMA harvesters

It is not yet possible to fully automate the harvesting of vegetables and lettuce. But subsequent work such as washing, weighing and packaging can be done directly in the fields, as a result of which the  process is speeded up considerably – so that very fresh products are then available to consumers. This task is carried out by special machines from Josef Zeyer GmbH. In the fields, the impressive machines can be controlled with a remote control unit connected to the vehicle by means of chainflex cables from igus.

Profile

  • What was needed: ready-to-install chainflex cable sets for energy and signal transmission
  • Requirements: UV and moisture-resistant, torsional resistance, temperature stable, notch-resistant & low wear
  • Industry: agriculture, special harvesters
  • Success for the customer: time and cost savings compared to internal assembly as well as long service life and flexible handling of the cables used
Harnessed readycable in ZEMA harvesting machines The harvesting machines from ZEMA allow a semi-automatic harvesting and processing operation right in the field. (Source: Josef Zeyer GmbH)

Problem

Josef Zeyer GmbH builds harvesting machines for vegetables and lettuce, which are always designed and manufactured according to customer specifications. The mobile machines reach an impressive size of up to 10 x 9 metres (when extended), so that the just-harvested produce can be processed as quickly and freshly as possible. The harvest is washed, portioned, packed and palletised manually by staff from a bridge whilst still in the field. It then travels via a conveyor belt to the inside of the harvesting vehicle, where it can then be further processed.
The machine travels in the field at around 40 metres per hour, either automatically or sensor-controlled in 'platooning' mode behind a tractor. However, the driver must still be able to readjust, for which - as well as for turning at the end of the field - he uses a wired remote control. In addition to the drives and steering, which are controlled electronically via CAN bus, the level control, i.e. the distance between the harvester and the ground, is also controlled via remote control.
It is true that the flexible cable connecting the remote control and the vehicle does not have to perform a high number of cycles or extreme movements. Nevertheless, the stresses and strains should not be underestimated. The cables are exposed to UV rays and moisture, but in particular to various torsions and very different temperatures. And, as they are often pulled along the ground, the amount of wear increases.

Solution

Since conventional cables do not meet the ZEMA requirements for service life, the company basically uses chainflex cables from igus for remote controls. The chainflex cables have a completely different design than those for static applications: the principle of cores wound in bundles ensures that the tensile and compressive forces acting on the individual cores during movement are balanced. This creates an essential prerequisite for a long service life in moving applications - without broken cores and corkscrews. The high-quality materials and the special extrusion process prevent further causes of failure, such as jacket abrasion and insulation damage.
Twistable chainflex cables from the CFROBOT9 series are used in the ZEMA machines. The cables achieve a long service life in the field and make the handling of the remote control easier as they are flexible and therefore more mobile.
ZEMA purchases the cable sets as a ready-harnessed energy supply. This has the advantage that the customer saves a lot of time and does not have to keep plug-in connectors or other accessories ready. And despite the commitment to one standard, Josef Zeyer GmbH remains flexible because the harnessed cables can be ordered in different lengths.

"We have had great experience with these cables. They achieve a long service life in the field and make the handling of the remote control easier as they are flexible and therefore more mobile."
 
Andreas Zeyer, CEO of Josef Zeyer GmbH
Remote control The machines move at around 40 metres per hour and in the field can be readjusted or operated by remote control.
chainflex CFROBOT cable The chainflex CFROBOT cables were specially developed for flexible applications. They therefore achieve a significantly longer service life - not only in harvesting technology.

Consulenza

Sarò lieto di rispondere di persona a eventuali domande

Spedizione e consultazione

Personalmente:

Dal lunedì al giovedì, dalle 8:00 alle 17:00.
Venerdì dalle 8:00 alle 16:30

Online:

24h


I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH