Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
Mon interlocuteur
Sélectionner un département

Indiquez-nous votre code postal, et nous vous dirons aussitôt lequel de nos collaborateurs pourra vous aider.

CH(FR)

Precisely adjustable plastic plain bearings in surgical lights from TRUMPF

TRUMPF iLED surgical light

TRUMPF Medical Systems

The TRUMPF iLED surgical light enables the adaptation to individual surgical operation situations.
The motor-powered swiveling LED wings are adjusted with the aid of JVFM-0810-08.

Advantages:

Clearance-free

Noise-free operation

maintenance free

Hygienic

Profile

  • What was needed: iglidur plain bearing technology
  • Requirements: Clearance-free and quiet operation, high hygiene requirements, lubrication and maintenance-free function.
  • Industry: medical equipment
  • Success for the customer: The iglidur plain bearings work reliably and without external lubrication. Due to the low friction coefficients in dry operation and the very low stick-slip tendency, the system is quiet and enables precise adjustment of the surgical lights.
Discover all products for medical technology
iLED operating light from TRUMPF

Problem

The TRUMPF Group is a renowned manufacturer of machine tools. However, the company also covers other sectors, such as medical technology. In the field of surgical lights, TRUMPF develops and produces the iLED series, which features innovative concepts, long-lasting LED technology, adjustable colour temperatures, integrated camera technology or shadow correction.
Another important feature of such surgical lights is the motorised, flexibly adjustable LED wings, which are designed to provide the best possible illumination of the patient during surgery.
For the pivoting movement, plain bearings are required which, especially in the highly sterile environments in which the surgical lights are found, are subject to the highest demands in terms of hygiene and freedom from lubricants. Likewise, they must always function reliably and maintenance-free.

Solution

This task is fulfilled today by preloaded bearings made of the high-performance material iglidur. Like all bearings from the iglidur product range, they work reliably over the long term without any external lubrication and are therefore maintenance-free. In addition to long service life, the bearings also stand for maximum comfort in terms of noise development. So that the surgeon can concentrate fully on his work, there is no cause for distraction whatsoever from the moving components of the surgical lights. Here, the very low coefficients of friction in dry operation and the very low stick-slip tendency benefit the operating room staff. The clearance-free arrangement of the plain bearings was also required here in order to ensure precise and problem-free adjustment of the luminaires at any time according to the user's wishes.



Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH