Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Il mio contatto
Seleziona luogo

Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.

CH(IT)

Extra-strong plain bearings in oscillating axle for semi-trailers

Maintenance-free, lubrication-free bearing points thanks to iglidur and igutex plain bearings

Profile

What was needed: 
Plain bearings with and without flange, thrust washers

Requirements:
Highly resilient, weather-resistant, lubrication-free / as little maintenance as possible

Industry: 
Commercial vehicles

Success for the customer: 
Lubrication-free bearing points that make maintenance easier for the end customer.
Oscillating axle for semi-trailers

Problem:

Bronze bearings were initially to be used in the oscillating axles of the semi-trailer. However, as these require additional lubricants, maintenance and servicing would have become very time-consuming. 

Solution:

The use of iglidur G plain bearings and thrust washers made of the heavy-duty material igutex TX1 made the use of additional lubricants superfluous and thus reduced maintenance and servicing to a minimum.

Excavator with pulley module

Working at a depth of 65 metres

One product Demarko develops is an oscillating axle for an articulated lorry trailer. Bearing point lubrication poses a particular challenge. A central lubrication system would increase production costs. So the design engineers were looking for an alternative that requires no additional lubricants. Now they use lubrication- and maintenance-free iglidur G plain bearings and igutex TX1 thrust washers.

Articulated trailers are used to transport oversized and particularly heavy objects. Trailer design and function ensure uniform wheel pressure distribution on the road surface, regardless of bumps. But they are not in continuous use like ordinary cargo trailers. For instance, they are sometimes exposed to the weather for months without the bearing points being moved or lubricated. Lubricated bearings would make the maintenance and repair of all bearing points in the oscillating axles cumbersome and time-consuming and therefore unattractive for the end customer. So Demarko was looking for a lubrication-free alternative.

Used in underground railway construction

The excavator with pulley module is used, for example, in the construction of underground railway lines that pass underneath the already existing underground railway network. It is therefore used in urban areas and must therefore be as compact and easy to transport as possible. In fact, the dimensions in the transport position with the hose reels folded in are identical to those of the conventional excavator.
 
With its grab, the excavator can move large quantities of earth out of the underground tunnels and load a whole 5 tons of material in one swoop. Loads and forces acting on the machine are thus considerable. Added to this are the weather, strong vibrations and dust. The operating conditions for all components are therefore demanding.


I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH