Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
Mon interlocuteur
Sélectionner un département

Indiquez-nous votre code postal, et nous vous dirons aussitôt lequel de nos collaborateurs pourra vous aider.

CH(FR)

Long service life in the production of wooden pallets with lubrication-free linear bearings

Aloysius Krenzer KG manufactures Europool pallets and customer-specific wooden pallets with a high degree of automation. When the technology experts in the company order new systems, they contribute their real-life expertise - and also influence the system manufacturer to use drylin linear guides for certain applications. The reason is that dry-running bearings prove their worth in linear drives that operate highly dynamically under heavy loads.

Profile

  • What was needed: linear guides in the drive and handling units of the pallet production systems
  • Requirements: resistance to chips, dust, moisture and resin, dynamic movements, vibrations and alternating loads
  • Industry: wood-working industry
  • Success for the customer: compared to conventional ball bearings and recirculating ball bearing guides, Krenzer achieves significantly longer service lives with dry-running drylin linear guides. In combination with hardened steel shafts, the pillow blocks work precisely and maintenance-free even under unfavourable environmental conditions.
Krenzer pallet production system

drylin pillow blocks

Completely lubrication-free with identical dimensions to recirculating ball bearing systems
Discover now

Free sample

Order your drylin R round-shaft sample and convince yourself of the quality
Order now!

Problem

Components in pallet production systems are exposed to special loads. These include wood chips and dust, moisture and resin. In addition, the dynamics of many drives are high, with 50,000 strokes per day. This applies, for example, to the handling units of the nailing station. The linear guides must be able to withstand alternating loads in a dusty environment as the moving ends attached to the axes move up and down when they remove a board from the storage. Added to this are the continuous vibrations caused by nailing.

The designers were dissatisfied with conventional bearings, such as ball bearings and recirculating ball bearing guides, as they did not help achieve convincing service lives.

Solution

After tests with different bearing types, drylin linear bearings proved to be the best solution. They allow for the longest service life, which is around three months. At first, that doesn't seem like much. However, if you multiply 50,000 strokes by 90 days, this results in 4.5 million working cycles and that in combination with dirt, high dynamics and alternating loads. The linear housings are equipped with liners made of wear-resistant iglidur J plastic and, thanks to the incorporated solid lubricants, do not require any external lubrication. As a result, no dirt sticks to them, maintenance is superfluous and the axes are guided with extreme precision.

Krenzer is so convinced by the dry-running bearings that they are not only used on the removal units for the cover boards from the storage, but also for the feeding and exact positioning of the cover boards. 
 

"In our experience, the drylin linear guides achieve the longest service lives with the frequent dynamic movements in our handling and feeding units."

Gregor Krenzer, Managing Partner of Aloysius Krenzer KG

Krenzer pallet production system with drylin pillow blocks Dust, chips, dynamic movements and alternating loads: these are the conditions under which drylin linear guides must prove their worth in the pallet production systems at Krenzer.
Krenzer pallet production system with drylin pillow blocks The drylin pillow blocks are also used for the feeding and exact positioning of the cover boards.
Krenzer pallet production system with drylin pillow blocks drylin linear guides with snow shovel effect, clearly visible here at a feeding station.


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH