Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Il mio contatto
Seleziona luogo

Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.

CH(IT)

Linear bearings for simple filling level adjustment in folding and gluing machines

Light, lubrication-free, robust: simple and reliable format adjustments in packaging machines

Nowadays, product information is increasingly easily obtained from the Internet. This also applies to machine components and purchased parts in order to save process costs. When designing customer-specific folding box gluers, the special machinery manufacturer Bernhardt Maschinenbau oHG relies on lubrication-free and maintenance-free linear plain bearings.

Profile

  • What was needed: drylin W linear rails, drylin T profile rails, drylin SLW lead screw linear systems
  • Requirements: Simple format adjustments, robust and maintenance-free components that must work lubrication-free due to cellulose in the air
  • Industry: Packaging industry
  • Success for customers: The lightweight and lubrication-free plastic creates flexible system modules. The drylin linear technology works reliably over the long term, even in two and three-shift operation.
Folding and gluing machine

Problem

One of the focal points of Bernhardt Maschinenbau oHG is the design of the folding and gluing machines. These are suitable for processing materials between 180g/m² and 600g/m². For example, the machines can be used to fold and glue CD covers, digi-packs, folding boxes, flight ticket bags or presentation folders at a speed of up to 300m/min. Due to their modular design, additional order and dispensing systems can also be connected at a later date and used flexibly. Customer requests are quickly addressed; for example, the manufacturer now offers a fast filling level device with a capacity of up to 5,000 cycles per hour. A prototype plant for 250,000 boxes was built, which must be able to quickly and easily adapt to new requirements for machine operators. Environmental conditions are also not always easy. Because paper contains cellulose. The ubiquitous paper dust, combined with humidity, can quickly combine to form a sticky mass that could disrupt the process. Robust and, above all, maintenance-free technology is therefore important.
In order to avoid production downtimes and unnecessary downtimes of the folding and gluing machines, high demands are placed on the machine elements used. Freedom from maintenance and lubricants, resistance to dirt, a long service life and, of course, economic efficiency play a very important role.

Solution

In the adjustment units of special attachments, the company relies exclusively on drylin linear plain bearing systems. Since the machine frames are not always in one place at the customer's site, plastic, which is very light in comparison, scores higher points compared to the steel guide. There is also the appearance. The system profiles are the same in all folding/gluing machines. The aluminium frame and the aluminium rail material of the drylin linear bearings harmonise in shape and colour. Another decisive factor was the price, which convinced the plant manufacturer just as the cleanliness of the lubrication-free bearings that prevent contamination of the product in the machine.
Even with maximum capacity utilisation in two and three-shift operation, the systems run smoothly today. Flexible drylin W guide systems with a linear lead screw or combined as a compact drylin SLW lead screw linear system are used in the filling level devices. In addition, robust drylin T profile rail guides prove their strength. The iglidur J has proven itself as a material in all cases. It was specially developed for linear applications in connection with hard-anodised aluminium surfaces.
In a current project, a silicone paper dispenser, the drylin W has likewise proved itself. With the dispenser system, up to 10,000 siliconised paper strips can be applied in a position precisely per hour. The dispenser is installed, among other things, in folding/gluing machines and is used for the production of cardboard shipping envelopes, for example. With a maximum space requirement of 10mm, a large number of axes are fitted with linear plain bearings. With them, the required speeds of 40m/min, which can be extended to up to 150m/min, can be achieved completely without any problems over very short distances.
“On the one hand, we were impressed by the price of linear plain bearings. On the other hand, cleanliness is important when handling paper and cardboard. Due to the absence of lubricants, nothing can drip and contaminate the product."

Max Steiner, Head of Design at Bernhardt Maschinenbau oHG

Folding and gluing machine
Folding and gluing machine
Folding and gluing machine
Folding and gluing machine


I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH