Indiquez-nous votre code postal, et nous vous dirons aussitôt lequel de nos collaborateurs pourra vous aider.
When the "Zoom" is on the road, it is only 3.90 metres long, making it a true compact caravan. Once at the campsite, the caravan can simply slide the entire sleeping section out over the trailer coupling via an electric motor and then gains not only 1.32 metres more usable length, but an alcove with a highly spacious double bed of 1.60 x 2.05 metres, which is neither in the way of the seating arrangement nor the kitchen.
But the sliding alcove is by no means the only innovation of the "Zoom". The kitchen concept is equally well thought-out and new. It is located in the rear and can easily be transformed into an open-air kitchen by swinging open the large tailgate. Ross Design has designed a movable kitchen unit that moves on two lateral lead screw axes in the vertical axis. If you want to cook outside, simply move the kitchen down a little. And if you raise the kitchen block all the way up, you can load bicycles or canoes through the large tailgate.
For the linear systems for the alcove and kitchen, the manufacturer needed both compact systems that could be easily integrated into the caravan and solutions that were as lubrication-free as possible.