Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
Mon interlocuteur
Sélectionner un département

Indiquez-nous votre code postal, et nous vous dirons aussitôt lequel de nos collaborateurs pourra vous aider.

CH(FR)

Linear bearings for track and tunnel cleaning

Lubrication-free drylin® linear bearings with high rigidity were required for this tunnel-cleaning vehicle.

Lorry or locomotive, rail or road? Owners of a work machine from ZWEIWEG International GmbH & Co. KG benefit from the double use of their vehicle. In the near future, the company will deliver a two-way cleaning vehicle for the metro in Riyadh, Saudi Arabia, which stands out due to its particularly flexible cleaning technology. Linear systems from our modular construction kit also contribute to this.

Profile

  • What was used: drylin® R aluminium shafts and pillow blocks,  drylin® W double rail and linear carriage
  • Requirements: lubrication- and maintenance-free components that are compact and yet provide a high reach for thorough cleaning of tracks and tunnels. They also have to be highly rigid and resistant to dust and dirt.
  • Industry: railway technology
  • Success for the customer: The lubrication- and maintenance-free drylin® linear technology is compact when retracted and yet allows for a long extension length that does not yield too much under the high water pressure. As it is lubrication-free, dirt and dust do not affect its functionality.
To the online shop

Problem

ZWEIWEG International GmbH & Co. KG develops and manufactures special vehicles that can travel on roads and rails. They are usually based on lorries and equipped with rail undercarriages, and are used, for example, for cleaning, overhead line and track construction or tunnel rescue.
For the commissioning of a third metro line in Riyadh in Saudi Arabia, such a cleaning vehicle was needed for both the track bed and the tunnels. The challenge: the tracks of the metro in Riyadh are not in gravel but slightly elevated in a concrete trough, and require a particularly flexible cleaning solution with movable cleaning arms.
For example, a large high-pressure unit with rotating nozzles for cleaning the tunnels is installed behind the driver's cabin and can be extended and moved. Furthermore, a suction arm at the rear of the vehicle must also be movable so that in can plunge deep into the concrete trough of the track bed. Finally, a construction of altogether eight arms arranged in the shape of a star, each equipped with five nozzle tips, had to be flexibly movable for tunnel cleaning.
For all these movable components, the manufacturer was looking for components that operate absolutely without lubrication maintenance, are as compact as possible and still allow a long reach when pushed out. In particular, the high back-pressure during cleaning with water required bearings that are extremely rigid and do therefore not yield. Even large amounts of dust and dirt in outdoor use should not cause any problems for the solution.

Solution

The suction arm at the rear, which is to be immersed in the concrete trough of the track bed, travels on a combination of pillow block and supported aluminium shaft of the series drylin® R from our linear technology program Although ZWEIWEG has a high level of vertical integration, our catalogue products were used here, which were convincing in terms of price and because they don't require lubrication or maintenance. The linear drive receives the control commands from sensors that scan the track bed and cause the suction arm to move up when they detect obstacles.
For the eight arms for tunnel cleaning, which are arranged in the shape of a star, the designers decided on two double shaft profiles of the drylin® W series, each connected back to back and driven by the on-board pneumatics. The system is very compact at rest and has a long range when pushed out. It also provides the necessary rigidity to withstand the back pressure of high-pressure cleaning - and it is resistant to water. In addition, the bearings easily compensate for tolerances in the vehicle and are insensitive to dust and dirt. 
The conclusion was correspondingly positive: with this project, the engineers realised a two-way cleaning vehicle that enables a 360o cleaning of track beds, tunnels and stations under special conditions.

Products used


"We generally work with a very high level of vertical integration - even for detailed designs. In this case, however, the catalogue products from igus are simply better and more cost-effective. Due to the combination of high-performance plastics and anodised aluminium, they are also free from maintenance and lubrication - simply perfect."

Dipl.-Ing. Oliver Paul, Sales and Project Planning at ZWEIWEG
drylin R linear rail Picture 2: The movable sensor-controlled suction arm takes over the cleaning of the track bed. The sliding suction arm is guided in a drylin® R linear system. The bearing easily compensates for tolerances in vehicle construction.
drylin W linear system Picture 3: The rotary nozzles for tunnel cleaning can be extended. Two drylin® W linear systems arranged "back-to-back" provide the linear motion. Good to see: the combination of aluminium guide and pillow block with plastic sliding element.


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH