Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Il mio contatto
Seleziona luogo

Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.

CH(IT)

The plastic energy chain guides 200kg/m cables on an offshore drilling vessel

A robust plastic e-chain ensures safe cable guidance for an offshore drill skid

This 3000HP modular offshore drilling rig has the world's largest plastic e-chain installed on a cantilever and the drill floor. Both energy chains were pre-assembled at our plant in Cologne so that they could be installed quickly on the drilling platform. Both travels (17.5m for the cantilever and 8m for the drill floor) bear an additional load of about 200kg/m.

Profile

  • What was needed: E4.1 series energy chains
  • Requirements: Given the 17.5m and 8m travel of cantilever and drilling floor skid, respectively, a safe cable guidance system for an additional load of 200kg/m was needed.
  • Industry: Oil and gas
  • Success for the customer: The plastic energy chains are designed to be strong and lightweight at the same time. This reduces the system's total weight. It is also particularly suitable for environmental conditions at sea (corrosion, wind, etc.)
Offshore energy chain Superlative energy chains: Despite high cable weights and enormous dimensions, the robust plastic energy chains safely move the drill floor skid and cantilever.

Problem

Modular drilling rigs are required for such situations as when drilling equipment needs to be added to fixed drilling platforms.
Mobile drilling vessels have all the necessary equipment for mooring at the drilling station and precisely placing the extended drill pipe. For this purpose, a huge cantilever moves over the drilling platform over which the drill pipe is finally to be set up and precisely positioned. Large cable guidance systems are required to ensure that the entire movable structure for setting up and placing the equipment can also move smoothly and without failing. In this application, the cantilever should be able to travel 17.5m, the mobile drilling floor 8m. The moving cables reach an additional load of 200kg/m, a major cable guidance challenge. The harsh conditions at sea meant that the solution needed to be particularly robust and durable, withstand corrosion, and have as little dead weight as possible.

Solution

Two of our E4.1 series plastic energy chains are used today to safely move the cantilever's cable load. Specifically, the E4.350 e-chain was chosen. It is the largest plastic energy chain installed on a cantilever and drilling floor.   It is not only strong, but also designed to use installation space optimally. This reduces weight and the drive energy required on the drilling rig. The heavy duty chains handle the heavy weight of the cantilever cables without any problem. Good preparation is also important for implementing such a project: Both energy chains were pre-assembled at our plant in Cologne so that they could be installed quickly on the drilling platform.
Offshore energy chain The chain could be installed quickly on the drilling vessel because the cable guidance system had been pre-assembled at our plant in Cologne.
Offshore energy chain The heavy cables on the drilling vessel required a particularly robust guidance system. This results in additional loads of about 200kg/m.

Here you can find the products used

E4.350 series

Inner height hi: 350mm
Inner widths Bi: 400-800mm
Bend radii R: 500-1000mm
Pitch: 470mm

Consulenza

Sarò lieto di rispondere di persona a eventuali domande

Spedizione e consultazione

Personalmente:

Dal lunedì al giovedì, dalle 8:00 alle 17:00.
Venerdì dalle 8:00 alle 16:30

Online:

24h


I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH