Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.
Site: engine plant in Austria. Application: indoor linear robot for the automated handling of engine blocks. At the engine plant in Austria, the largest and most important engine plant of a major German car manufacturer, an engine comes off the assembly lines every 14 seconds on average - at peak times more than 6,000 engines are produced each working day. This extremely high output can only be achieved with a high degree of automation and with extremely reliable components. The goal of the operators is to always avoid failures and system downtimes if possible. These high standards were therefore also set for the energy supply system of the indoor gantry. In fact, this later has to work continuously in 18 to 19 shifts per week with high dynamics. Future energy supplies can quickly reach cycles in the millions.