Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Il mio contatto
Seleziona luogo

Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.

CH(IT)

Robust plastic energy chains in a tunnel boring machine

A tunnel boring machine moves deep slowly through the earth. The entire tunnelling machine is exposed to mechanical loads, dirt, moisture and sometimes high temperatures. A number of harnessed plastic energy chains are used for the energy supply for the segment lining and in material handling. They are exposed to conceivably harsh environmental conditions in a small installation space.

Profile

  • What was needed: E4.1 energy chain system, E4/4 series energy supply systems with reverse bend radius (RBR), chainflex signal and high-voltage cables
  • Requirements: continuous operation, harsh environmental conditions with high load level
  • Industry: Tunnel boring
  • Success for the customer: harnessed chainflex solution with energy chain and cables saves assembly time, durable and strong energy supply solution ensures failure-free project sequence
Tunnel boring machine

Problem

The tunnel boring machines from Herrenknecht AG, Schwanau-Allmannsweier are always tuned to their respective tasks and geological and hydrological conditions.  In 2010, Herrenknecht was commissioned to build a tunnel boring machine (TBM) in order to build a traffic tunnel, "the Port of Miami Tunnel", in the port of Miami. This was to ease the traffic of almost 16,000 vehicles every day that clog the roads to and from the cruise and freight port in Miami.  The solution: a Herrenknecht tunnel boring machine of the "earth pressure shield" type.  The entire machine has a weight of 2,500 t; its length is 110 m.  While all tunnel boring machines are custom-built, the one thing they all have in common is that they are usually in almost continuous operation from the day of commissioning until they breakdown, which entails high demands on load resistance, also in terms of the energy supply systems. These are needed because a whole range of different crane systems are used in the tunnel boring machine for a wide variety of tasks.  These are the material handling cranes which transport for example pipes, cable drums and other workshop equipment from the utility vehicles to the respective application site. "These cranes for pipe laying, cable drums and workshop equipment play an extremely important role in the overall process," explains Dietmar Stahl, team leader for crane construction for traffic tunnelling. "They are responsible for the respective supply." For the extension of the conveyor belt, a workshop crane or conveyor material crane is subjected to the heaviest use.

Solution

All the above crane systems are equipped with two or three harnessed energy supply systems from igus for longitudinal and transverse travel. One is the energy chain system E4.1, which can be opened from both sides, and is very robust and protects the inserted cables.
Not only in material handling, but also in the erector, which is responsible for placing the tubbing, robust energy supply systems prove their strength. For the tubbing segment lining, immediately after the drilling process, the tunnel is supported permanently with the tubbings in the form of a ring to protect the shield skin. The tubbing segments are positioned on the tunnel wall by means of an erector, a remote manipulator, held mechanically or by vacuum, and then screwed. The erector's radius of action of +/-200° is achieved with energy supply systems of the E4/4 series with reverse bend radius (RBR) and an installation position turned by 90°.
E4/4 chains are characterised by high stability and torsional strength. They can be opened from both sides and equipped with various mounting brackets. Long unsupported applications, also mounted on the side, are implemented just as reliably as gliding applications. The e-chain series proves itself especially in harsh environmental conditions.
In addition, a harnessing with bending-resistant chainflex signal and high-voltage cables from igus was carried out.
Tunnel boring machine
energy chain

Harnessed complete system readychain as a success factor

Not only the driving machine itself, but also the components in the background had to be designed precisely for the respective requirements on site, so that the tunnelling work could take place within the given time frame. As described above, this applied to a large extent to the energy supply systems of the series E4.1 and E4/4, which have proven themselves in the crane systems and, above all, in the erector, directly behind the drill head, despite the huge dirt accumulation. "Durability and stability play an extremely important role", says Dietmar Stahl. "The energy chains of igus convince us due to their material and design. We have been working together very successfully for several years." The Miami Mammoth project also includes the harnessing with the flexible chainflex signal and high-voltage cables. Dominik Küntzler: "That way, we save a lot of assembly time, among other things. " Even if only a small amount of installation space is available, all cables are protected. The switch cabinet can be installed separately. "This gives us the flexibility we need for this complex task."
energy chain


I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH