Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Il mio contatto
Seleziona luogo

Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.

CH(IT)

Safe, flexible cable guidance for KUKA articulated arm robots in aircraft construction

Airbus subsidiary uses triflex R and E4/4 plastic energy chains on axes 1 to 7

A KUKA robot suspended from the ceiling for aircraft component construction was to be equipped with various cable guidance systems on axes 1 to 7. Supply of energy and data was to be reliably provided during the articulated arm robot's complex rotary and pivoting movements and vertical strokes. The core of the solution today is a triflex R energy chain that flexibly follows the robot arm on axes 2 to 6. A robust E4/4 energy chain also allows lifting over a 5m travel and allows the system to rotate 380°.

Profile

  • What was needed: triflex R 3D energy chains; E4/4 energy chain
  • Requirements: failure-free supply of a KUKA 125 - 2 with energy and data on axes 1 to 7
  • Industry: aircraft construction
  • Success for the customer: The triflex R flexibly follows the complex movement of the articulated arm robot. A defined bend radius enormously increases the service life of the guided cables and hoses beyond what a cable protection hose allows.
Products for aviation and aerospace
KUKA robots This KUKA articulated arm robot is used in CFRP processing in the aviation industry. A solution was to be found for cable guidance on axes 2 to 7 and for robot lift and rotation.

Problem

As in the automotive industry, everything in aircraft design is based on tight schedules. So it is not surprising that the failure of an expensive machine or a robot not only greatly delays processes, but also means high costs.
For KUKA articulated arm robot cable guidance, CTC-GmbH, a subsidiary of aircraft manufacturer Airbus, was concerned with just this issue. Within the Airbus Group, the company specialises in manufacturing development for carbon fibre reinforced polymer processing (CFRP). For particularly lightweight alternatives to milled metallic components, special processes are being developed to reliably produce even load-bearing parts of the aircraft fuselage with cutting-edge carbon fibre technology.
This is just where the robot in question, a KUKA 125 - 2, comes in. Its tool needed to be supplied with energy and data to perform its tasks.

Solution

Since the robot was also to be equipped with a seventh axis and rotates around its own axis, we delivered several energy supply systems to the Airbus subsidiary.
The key component of the cable guidance solution today is a triflex R energy chain for axes 2 to 6, which move three-dimensionally, that is installed directly on the robot arm. The 3D energy chain flexibly handles the industrial robot's complex, jerky rotational and pivoting movements. A defined bend radius also enormously increases the service life of the guided cables and hoses beyond what a cable protection hose allows.
For the linear motion on axis 7, we recommended installing an E4/4 energy chain on a travel of 5m. The especially versatile cable guidance system is easy to install and has a modular design. In this application, the solution meets the need for an especially robust chain with high rigidity.
The cable guidance for the KUKA robot is rounded off with another E4/4 energy chain for the robot's circular movement on the first axis. This allows rotation of 380°.
KUKA articulated robot The hanging KUKA robot can be rotated 380°. This is accomplished with an E4/4 energy chain on the first axis.
KUKA articulated robot

More on applied products here

Further interesting applications from extremely diverse areas can be found here.



I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH