Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Il mio contatto
Seleziona luogo

Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.

CH(IT)

Quiet, low-vibration energy supply system for a dynamic machining centre

Quiet energy chains with high acceleration in machines from traditional companies

Direct drive technology is also becoming increasingly popular in machine tool construction. Non-productive times and set-up costs are further reduced and machining speeds increase. Following the appropriate on-site consultation, a traditional company has equipped its two-spindle horizontal machining centre with exceptionally quiet and low-vibration energy supply systems that easily cope with the technical requirements for dynamics and acceleration.

Profile

  • What was needed: E6 series energy chains
  • Requirements: detailed technical advice due to the demanding system, low space requirement, sensible arrangement of the cables within the chain, high travel speeds and accelerations
  • Industry: machine tool manufacturing
  • Success for the customer: detailed and individual advice led to the use of the E6 series, which impresses with its exceptionally long service life, extremely quiet and low-vibration operation and modular design; so far, no incidents have occurred despite heavy loads and high travel speeds
Discover all products for machine tools
energy chain The igus energy supply systems of the E6 series are extremely quiet and have low vibration. They prove themselves in the two-spindle horizontal machining centre. All axes here are equipped with direct drives.

Problem

"We designed this machining centre especially for aluminium and light metal machining, for smaller batches", explains Dipl.-Ing. Torsten Keller, a Design Engineer at Saalfelder Werkzeugmaschinen GmbH (Samag-Group), Saalfeld, Germany, since 1995. The two-spindle horizontal machining centre with linear drives 'MFZ 500 - 2 linear' in the 3-axis unit, additionally equipped with independent Z and A/B axes for 5-axis machining, is characterised by reduced non-productive times, increased accuracies, a generous clamping area for larger workpieces and multiple clamping solutions, as well as fast job changeover and high flexibility, thanks to the double pallet changing system. It is mainly used in the automotive supply industry for machining cubic parts.
"With our complex machines, it basically comes down to technical advice on the one hand to find the best solution. On the other hand, the lowest possible space requirement is a priority for the machines, so we are happy to take advantage of application support in the run-up to the design", says Torsten Keller. "It is also a question, amongst other things, of achieving a sensible arrangement of all the cables within the energy supply system. The multitude of electrical, hydraulic and pneumatic as well as data cables must be accommodated systematically, logically and in a space-saving manner."
Further requirements for the energy supply systems: they must be able to safely handle axis speeds of 100 or 120 m/min, accelerations of 1 to 1.5 g, spindle speed ranges of 50 to 15 000 min-1 and travels of 450 to 630 mm at all times. Lastly, a wide variety of coolants must be taken into account, which are used in the system and can corrode the individual components.

Solution

Energy supply systems from igus have been used for many years in almost all of the company's horizontal machining centres and special machines, precisely matched to the respective design requirements.
In the case of the linear machine, igus recommended the E6 series energy supply system. It displays its special strength especially with high-speed axles. Since 2005, it has been used in the two-spindle horizontal machining centre with linear drives and has been convincing right from the start. Despite the high stress in everyday operation, no failures of the energy supply system have been recorded.
In addition to its long service life, it also offers numerous other advantages. It is characterised by extremely quiet, low-vibration operation. It minimises the polygon effect which can occur during the rolling motion of an e-chain®. The extremely low noise emission (confirmed by an expert assessment report from TÜV Rheinland) is only 46 dB(A).
Another advantage is the modular design of the E6 energy chains: The energy supply system can be shortened and lengthened as desired. A characteristic feature is the elastic spring element made of plastic, which connects the individual side parts to form a very robust energy supply system. The scalable crossbar shows no signs of wear even after 220 million strokes in the endurance test. The absence of the usual pin/bore connection results in low-vibration and quiet operation.
The quiet and low-vibration energy supply system is matched to the high speed and acceleration values in direct drive technology and ensures a continuous and reliable supply of all necessary media - from energy and compressed air to control information - even over longer distances if required. "The technical advice was worthwhile for us in the overall concept right from the start," Torsten Keller concludes.
Energy chains View from above of the energy supply systems in the two-spindle horizontal machining centre.
E6 energy chain One advantage of the E6 energy chain is its modular design, which allows it to be shortened and lengthened as required.

Saalfelder Maschinenbau GmbH - A company with tradition

"We can look back on over 130 years of experience in machine tool manufacturing," reports Dipl.-Ing.-oec. Simone Stadermann, Assistant Sales Manager, about the Samag company history. At the Saalfeld site, the mechanical engineering division develops and builds two- and four-spindle horizontal machining centres for medium- and large-scale production. In addition, there are special machines and multi-spindle deep-hole drilling machines. "We see ourselves as a solution provider. Whether light metal or heavy machining tasks - our systems flexibly and reliably handle all customer-specific requirements," says Simone Stadermann.
In the second business area, Automotive, parts are machined for medium and large volume production. These are assemblies of the engine and transmission for the automotive industry. These include  axis housings, lids, bevel gears, differential compensation housings of axis gearboxes or also crankshaft bearing lids of the engine. "We use our own machining centres for the complete machining of the workpieces. This means that our customers benefit from the synergy effects of machine tool construction and parts production. In addition, we can demonstrate our machines and systems in action at any time," says Simone Stadermann. "From the field of practice and for the field of practice, they secure decisive competitive advantages!"


I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH