Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
Mon interlocuteur
Sélectionner un département

Indiquez-nous votre code postal, et nous vous dirons aussitôt lequel de nos collaborateurs pourra vous aider.

CH(FR)

From rotation to fun: e-chain circular module in the PowerSplash water ride

Load cables, signal cables and pneumatic hoses safely guided in the pivoting gate


At 100km/h and a drop of 45m, the "PowerSplash" launch coaster races through the water in the Walibi amusement park in Belgium. To ensure that passengers can board and disembark safely, the developers of the water ride from the company MACK Rides installed a pivoting gate, which made special demands on the energy supply. igus provided the right solution with a rotary module.
  • What was needed: guiding device for the load cables, signal cables and pneumatic hoses under the pivoting gate
  • Requirements: movement of the cables by +/-180°, suitable for high loads, long service life, minimum installation and maintenance requirements
  • Industry: amusement rides
  • Success for the customer: a modular igus rotating energy supply consisting of two vertical e-chains and a guiding device reliably moves the many cables in both directions. The system is robust and space-saving, is designed by our engineering specialists, delivered ready for connection and installed by us upon request.
RBR energy supply in the PowerSplash coaster from MACK Rides

Problem

The designers at MACK Rides equipped the PowerSplash with a pivoting gate as a station element between the station building and the roller coaster area. These stations allow passengers to get in and out comfortably while on the other side the next boat starts its ride on the actual rail. A suitable energy supply was needed for the many load cables, signal cables and pneumatic hoses. It has to be able to rotate the cables by 180° in both directions. The revolving platform has a diameter of 12.4m, is 4.9m high and, together with the two boats, has an impressive weight of 40 to 59t.

Solution

The igus engineering team provided the perfect solution: a modular rotating energy supply consisting of a double side-mounted energy chain in a guide rail. It ensures that the pivoting movement and the movements of the disc are implemented and guide the cables safely and without damage. With the help of specially shaped chain supports, any height offsets that occur during operation can be compensated for. To save time, money and effort, the PowerSplash designers opted for a ready-to-use harnessed readychain system, which our engineering team installed directly under the rotary disc.

Ready-to-connect energy chain systems such as the rotary module are designed, harnessed, assembled and tested at igus in Cologne. This means that the customer receives a system with a guarantee from one source.
PowerSplash water ride The PowerSplash is a launch coaster in which the boat is propelled forwards and backwards with over 2000HP until it reaches a drop height of 45m and 100km/h.
PowerSplash water ride A pivoting gate serves as an element of the station. While the passengers of one boat change, the second boat turns into the actual roller coaster rail.
RBR energy supply in PowerSplash water ride Compactly installed under the revolving platform: a rotary module with two energy chains from igus ensures reliable guidance of the many cables and hoses.

Rotating energy supplies

Overview of our energy supply systems for rotating applications. Maximum rotation angle in minimal installation space.
Find out more now

Products for fun rides

Safe movement, less maintenance: our energy supply systems and bearings for a wide variety of fun rides
Discover now


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH