Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Il mio contatto
Seleziona luogo

Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.

CH(IT)

Curved drylin® linear rails and energy chains for the rotation of igus® make monitors movable

An old water tower has been converted into the central control room for monitoring the water supply. The space in the upper part of this tower is used as a training centre that focuses on the environmentally friendly use of water resources and as a meeting room for the company management and its partners. As an aid for future training purposes, six movable television screens were set up in two rows, which move around the room in a radius of 6.8m and at an angle of 180°. In addition, there are another six movable television screens in the upper conference room, which are arranged in a single row. These television screens move in a circle with a radius of 5.9m and an angle of 45°.

Profile

  • What was needed: drylin W curved linear guide
  • Requirements: An arc movement with energy supply without interruptions in a 180 degree swing.
  • Industry: Waterworks
  • Success for the customer: Everything from one source - everything from curved rails to energy chains and ready-to-connect cable, came from igus
Do you need more information? Contact us here

Problem

At the beginning of the whole project we faced several challenges. Two of those challenges were:

1. How are the TV screens mechanically guided in a circular room?
2. How do we bring power and data supply to mobile TV screens?  

We also wanted to keep the maintenance effort as low as possible so that the scheduled meetings and training sessions would not have to be suspended for maintenance work. Thanks to the support of igus®, we did not have to search long for the individual components and were very happy to be able to get everything from one source.  
768 manus
768-manus

Solution

We worked out the solution together with igus®:
Curved rails in installation sizes 10-120-10 in order to guide the monitors on the round wall.
Carriage for curved rail WWB-10-120-10 - maintenance-free and lubrication-free with very quiet operation.
RBR energy chains 2400.03.100 & 2400.03.100 specially designed for rotating movements
In the Reverse Bend Radius energy chains we then installed the chainflex CF9.10.04, also manufactured by igus®, for the energy supply. For data transmission CFBUS.049 and CFPE.25.01 for the ground connection.We always had a contact person - igus® - and always found ourselves well advised. 

Products used

banner_curved_bends

drylin® W curved

 

  • Variable profile directions 
  • Suitable linear carriages
  • Lubrication-free drylin® W carriages for curved rails
  • More information
Buy here

More information

drylin W profile guide drylin W curved rails provide the guidance of the monitors. We could use the linear rail WS-10-120.
 
drylin curved rails
drylin WWB-10-120-10

Matching the curved rail, igus® was also able to deliver the carriages directly. WWB-10-120-10 - The larger version of the WWB-10-40-10 already available in the shop. 

Request WWB-10-120-10 here
Energy chains by igus

In addition to rails and carriages, igus also supplied the power supply for the monitors and the protective RBR energy chains.
 

Energy chains for rotating movements

Why choose drylin® W profile guides?

Robust

Less installation time

Quicker assembly thanks to double rails instead of two single rails mounted in parallel
Property icon

Great variety of materials

For a large number of applications (e.g. automation, food industry, medical technology, pharmaceuticals industry)
Property icon

More ergonomics

Curved rails provide more design freedom, for example in workstations
Property icon

Smooth running

Carriage with hybrid roller bearings for smoother running
Property icon

Weight-optimised

With extremely light carbon rail material
Property icon

More variability

in design thanks to flexible distances with parallel single rails



I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH