Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Il mio contatto
Seleziona luogo

Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.

CH(IT)

Energy chains and cables for fail-safe storage and retrieval units from viastore

Automated and highly flexible storage systems with chainflex special cables and energy chains

The importance of intralogistics is increasing worldwide. System providers such as viastore systems plan and implement automated storage systems – ranging from small parts and pallet warehouses to shuttle warehouses – including storage and retrieval units (SRUs). These must work quickly and flexibly in order to be able to react to changing order cycles and quantities. Users also demand fail-safe systems to avoid unplanned downtime. viastore relies on the flexible chainflex cables from igus to supply its storage and retrieval units with energy and data.

Profile user report

  • What was needed: Energy chains, chainflex cables
  • Requirements: Safety with fast stroke movements and vibrations, resistance to freezing
  • Industry: Mechanical engineering, small parts storage and retrieval units (SRUs)
  • Success for the customer: Savings of enormous  process costs and at the same time risk minimisation, because the components function perfectly, reliable and long-lasting solutions, which ensure high availability of the plant and keep maintenance costs low
Discover our products for intralogistics
Viastore storage and retrieval unit viastore SYSTEMS plans and implements automated storage systems - ranging from small parts to pallet and shuttle warehouses - including storage and retrieval units (SRUs). These must work quickly and flexibly in order to be able to react to changing order cycles and quantities.

Problem

Within intralogistics, providers organise internal material flows by means of technical systems and software solutions. An elementary component here are automatic storage and retrieval units (SRUs), which move goods and store them in and retrieve them from the compartments of the high-bay racking.
Since 1970, the Stuttgart-based company viastore has been developing and producing storage and retrieval units for all types of warehouses, in all size and speed classes, and differentiates between three basic types according to travel speed and payload. The smallest system, "viaspeed", has been specially designed for plastic containers and cartons and for a payload of up to 50 kg. With a travel speed of 6 m/s and an acceleration of 3 m/s², it is highly dynamic. The SRU "viaspeed XL", on the other hand, picks up loads of up to 300 kilograms and transports containers and trays. It has a travel speed of up to 5 m/s and accelerates vertically at 2 m/s2. The system can still be used at temperatures from minus 40 degrees Celsius to plus 45 degrees Celsius. Finally, the most powerful storage and retrieval unit, viapal, handles pallets, wire mesh boxes and other loads of up to three tons. The dynamic travel drive makes a travel speed of 3 m/s and a vertical acceleration of 1.5 m/s2possible.
These performances show that in all SRUs, whether small or large, the demands on the systems are very high. viastore offers solutions that are highly dynamic and flexible, allowing for increased number of retrieval and storage actions when the number of items and orders increases. Warehouse operators expect automated solutions to adapt to ordering processes and to respond faster to peak times. They also demand reliable and durable solutions that ensure high plant availability and keep maintenance costs low. Against this backdrop, it is crucial that all components in the units, such as the energy supply solution, also function superbly under precisely this high requirement profile and need to be maintained only rarely, if at all.

Solution

Today, these requirements are met by the maintenance-free polymer energy chains and chainflex cables from igus. They are installed in the lifting gear on the mast of the storage and retrieval units and supply the systems with energy and data like an umbilical cord. Especially the fast lifting movements and vibrations at large unit heights or at high travel speeds place an extremely high load on the cables. Conventional cables can often form corkscrews, which can lead to core breakage.
This is why igus began developing special cables under the brand name chainflex for dynamic use in energy chains back in 1989. A special feature is their specific structure consisting of cores wound in bundles. Here, the cores are not wound in layers around the centre of the cable, but are wound together in three, four or five cores, which are then wound together again to form a complete stranding of the bundles. Additionally, gusset-filling extruded inner jackets fill the spaces between the cores. The effect: The stranding cannot unravel and each core is moved equally in the inner and outer radius when moving in the energy chain. One-sided stretching and compression, which often lead to core ruptures or corkscrews, are a thing of the past.
But temperature-resistant cables are also important to viastore for use in deep-freeze warehouses. They have to cope with small bend radii and millions of strokes at very low temperatures. Not only the design principle but also the used materials qualify the cables for continuous use in this application. For example, in particularly cold ambient conditions, cables with specially developed highly cold-flexible TPE outer jacket materials are used.
But the variety of cable types in the igus range was also important to the customer. viastore can flexibly offer 1,244 chainflex cables – from control and servo cables up to motor and robot cables as well as bus, encoder and fibre-optic cables .

"We need to know what the expected service life of the chainflex cables is in order to be able to reliably plan the replacement cycles. Unplanned system downtimes must not occur under any circumstances. Therefore, we would like to be able to make statements to our customers about the durability of all components that are installed in our SRUs. "
 
Friedbert Dannenhauer, Deputy Head of Design at viastore on the relevance of the online service life calculation from igus
Energy chain and chainflex cables The maintenance-free e-chains and chainflex cables from igus are mounted in the lifting gear on the mast of the viastore storage and retrieval units and supply the systems with energy and data.
Energy chain and chainflex cables

Service life calculation makes maintenance plannable

igus gives a three-year guarantee on the chainflex cables. The company can offer this security because it tests all cables under real conditions. The test results flow into a database, on the basis of which the expected service life of the products is calculated, which every user can compute on their own in a time-saving way on the igus homepage. The basis for the service life calculator is the igus database, which has grown over decades and in which the results of thousands of tests from the test laboratory and decades of experience in the development and production of chainflex cables are stored. On this basis, the online tool calculates the expected service life of the chainflex cable. Otto Funk, Head of Design at viastore SYSTEMS, emphasises why this is so important: "We need to know what the expected service life of the chainflex cables is in order to be able to reliably plan the replacement cycles. Unplanned system downtimes must not occur under any circumstances. Therefore, we would like to be able to make statements to our customers about the durability of all components that are installed in our SRUs," says Friedbert Dannenhauer, Deputy Design Manager at viastore SYSTEMS. igus has developed a variety of other online tools to make it easier for the system integrator to select the right products, configure them and order them. Such additional services help to save time and reduce costs. The people in charge at viastore also appreciate this. Friedbert Dannenhauer and Otto Funk are not only satisfied with the chainflex cables from igus, but also with the service. "The advice from igus and the cooperation over the entire course of the project is really very good. The idea of partnership is always in the foreground," concludes Friedbert Dannenhauer.
Calcolatore della durata d'esercizio chainflex®
Test laboratory cold chamber In the cold chamber at igus, cables can be tested at temperatures from -40°C to +60°C.


I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH